Skip to main content
Adriano Melis
Associate III
November 7, 2016
Question

CubeMX error code generation

  • November 7, 2016
  • 5 replies
  • 1262 views
Posted on November 07, 2016 at 12:19

When regenerating code (previously correctly generated several times) CubeMX displays an error window and deletes an initialization assembler source file which prevents the Eclipse/System Workbench project to build successfully.

The text on the window says ''The Code is successfully generated under C:/..... but SW3STM32Project generation have a problem.''

The deleted assembly file is Drivers/CMSIS/Device/ST/STM32F0xx/Source/Templates/gcc/startup_stm32f051x8.s

I have attached the .ioc file for reference

#!cubemx-!code-generation
    This topic has been closed for replies.

    5 replies

    ST Technical Moderator
    November 11, 2016
    Posted on November 11, 2016 at 13:57

    Dear User,

    Please note that your issue is reported internally for checking and we will contact you soon.

    Best Regards

    STM32.forum

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Adriano Melis
    Associate III
    November 23, 2016
    Posted on November 23, 2016 at 11:08

    It happened again. I was using a new project which did not show the problem. Just after I checked the box ''Delete previously generated files when not re-generated'' CubeMX shows the same error window and deletes the assebnly initialization file. This is really annoying.

    Unchecking the box does not change the behavior of CubeMX: this .ioc can not be used in the same place anymore.

    Adriano Melis
    Associate III
    November 23, 2016
    Sirma Siang
    ST Employee
    January 27, 2017
    Posted on January 27, 2017 at 17:09

    Hello

    Melis.Adriano

    ,

    A similar bug has been fixed in 4. Since, the 4.19 has been released.

    Could you please try with that newest version ?

    Great thanks in advance.

    Kind regards

    Marc

    digital B
    Associate
    November 30, 2017
    Posted on November 30, 2017 at 23:45

    I can confirm this for version 4.19 too.

    This appears to be due to a missing .xml file that accompanies the .ioc file (it has the same name as the .ioc file).

    I found this out after renaming the .ioc file.

    Solution:

    a) Rename the .xml file as well

    or

    b) Undelete/recover the .xml file

    or

    c) Copy another such .xml file and edit it to fit the .ioc project (it contains project, MCU and debug interface name)