Visitor II
November 11, 2016
Question
Bad SPI clock duration in stm32f746
- November 11, 2016
- 2 replies
- 844 views
Posted on November 11, 2016 at 18:08
Hello. I have got stm32f746 and I make project with cubeMX.
I want to use SPI4, SPI5, SPI6 as fullduplex master with 50Mb/s baudrate. Then I try to HAL_SPI_Transmit(&hspi4, pData, 1, 30000); in while(1) cycle. Data has been sent, but the clock is very bad.(I put image in attachment. You can see there.) As you see, duration is not 50%. When I set baudrate less then 50Mb/s, may be clock is good, but I need only 50Mb/s. Is this my fault, or this is bug?