Skip to main content
ricardomadera
Associate II
November 18, 2016
Question

Workaround interfacing STM32F429 FMC with a TFT

Posted on November 18, 2016 at 16:39

Hello,

I am working with a smart TFT that supports the 8080 parallel interface on a custom board but the design omitted connecting the RD, RS, CS, WD to the appropriate NEx, NOE, NWE, Ax pins. Instead these 4 control lines are connected via regular GPIO.

I thought I could get away with managing the control lines manually, and letting the FMC do the work of reading and writing. I am able to write to D0-D15 just fine but reading always yields 0x0000. I think this is because the FMC controller isn't being toggled via it's pins to enter a reading state. 

Is there anyway to work around this limitation while still using FMC? Or will I have to control all the pins manually due to these 4 omitted connections? I might be able to cut traces and jumper my prototype, but I'm hoping there is an alternate method here. 

Any insight is appreciated. Thanks!

    This topic has been closed for replies.

    4 replies

    mark239955_stm1
    Visitor II
    November 19, 2016
    Posted on November 19, 2016 at 11:02

    If the additional control lines are free, i.e. not connected to anything else, you could try enabling their alternate functions to see if that makes reading start working.

    Better yet, if those control lines are not in use, just wire your bad choice pins to the right pins and make sure the bad choices are configured as digital inputs.  The small additional load is unlikely to matter.

    ricardomadera
    Associate II
    November 19, 2016
    Posted on November 19, 2016 at 15:50

    Hi Markt,

    Thanks for the idea. It does seem to work (as in not crashing) but i am still not getting a read. Before I cut up traces on this prototype to re-route the 4 lines manually, I decided to replicate the setup on the STM32F407 disco. I have the FSMC up and writing, but I am still not getting LCD reads. The control lines are being toggled correctly now so i'm trying to figure out what I am missing. All my code is very similar to the STM32F103 tft sample. 

    ricardomadera
    Associate II
    November 19, 2016
    Posted on November 19, 2016 at 19:03

    Ok so I managed to get the F407 Disco reading the panels ID. But oddly D10 ( PE13) is misbehaving. It reports an active high of 1/2 vcc or 1.5v. When outputting values it only reaches 400mv.. Is there something on the F4 disco drawing too much current?

    ricardomadera
    Associate II
    November 19, 2016
    Posted on November 19, 2016 at 19:12

    Here are my GPIO and FSMC inits 

    void LCD_CtrlLinesConfig(void)

    {

    GPIO_InitTypeDef GPIO_InitStructure;

    /* Enable GPIOD, GPIOE, GPIOF, GPIOG and AFIO clocks */

    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD |  RCC_AHB1Periph_GPIOE |

    RCC_AHB1Periph_GPIOF, ENABLE);

    /*-- GPIO Configuration ------------------------------------------------------*/

    /* SRAM Data lines,  NOE and NWE configuration */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_8 | GPIO_Pin_9 |

    GPIO_Pin_10 | GPIO_Pin_14 | GPIO_Pin_15 |

    GPIO_Pin_4 |GPIO_Pin_5;;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

    GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_NOPULL;

    GPIO_Init(GPIOD, &GPIO_InitStructure);

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource0, GPIO_AF_FSMC); //D2

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource1, GPIO_AF_FSMC);//D3

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource4, GPIO_AF_FSMC);//RD/NOE

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_FSMC);//NWE/WR

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_FSMC);//D13

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_FSMC);//D14

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource10, GPIO_AF_FSMC);//D15

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_FSMC); //D0

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_FSMC);//D1

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource7, GPIO_AF_FSMC);//CS - NE1

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 |

    GPIO_Pin_11 /* //RST*/ | GPIO_Pin_12  /*RS/A17*/| GPIO_Pin_11 | GPIO_Pin_14 |

    GPIO_Pin_15;

    GPIO_Init(GPIOE, &GPIO_InitStructure);

    GPIO_PinAFConfig(GPIOE, GPIO_PinSource7 , GPIO_AF_FSMC);

    GPIO_PinAFConfig(GPIOE, GPIO_PinSource8 , GPIO_AF_FSMC);

    GPIO_PinAFConfig(GPIOE, GPIO_PinSource9 , GPIO_AF_FSMC);

    GPIO_PinAFConfig(GPIOE, GPIO_PinSource10 , GPIO_AF_FSMC);

    GPIO_PinAFConfig(GPIOE, GPIO_PinSource11 , GPIO_AF_FSMC);

    GPIO_PinAFConfig(GPIOE, GPIO_PinSource12 , GPIO_AF_FSMC);

    GPIO_PinAFConfig(GPIOE, GPIO_PinSource13 , GPIO_AF_FSMC);

    GPIO_PinAFConfig(GPIOE, GPIO_PinSource14 , GPIO_AF_FSMC);

    GPIO_PinAFConfig(GPIOE, GPIO_PinSource15 , GPIO_AF_FSMC);

    /* SRAM Address lines configuration */

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;

    GPIO_Init(GPIOF, &GPIO_InitStructure);

    GPIO_PinAFConfig(GPIOF, GPIO_PinSource0, GPIO_AF_FSMC);

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 ;

    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

    GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_DOWN;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

    GPIO_Init(GPIOD, &GPIO_InitStructure);

    }

    void LCD_FMCConfig(void)

    {

    FSMC_NORSRAMInitTypeDef  FSMC_NORSRAMInitStructure;

    FSMC_NORSRAMTimingInitTypeDef FSMC_NORSRAMTimingInitStructure;

      /* Enable FMC clock */

      RCC_AHB3PeriphClockCmd(RCC_AHB3Periph_FSMC, ENABLE);

    /*-- FMC Configuration ------------------------------------------------------*/

    /*----------------------- SRAM Bank 3 ----------------------------------------*/

      /* FMC_Bank1_NORSRAM4 configuration */

      FSMC_NORSRAMTimingInitStructure.FSMC_AddressSetupTime = 5;

      FSMC_NORSRAMTimingInitStructure.FSMC_AddressHoldTime = 0;

      FSMC_NORSRAMTimingInitStructure.FSMC_DataSetupTime = 5;

      FSMC_NORSRAMTimingInitStructure.FSMC_BusTurnAroundDuration = 0;

      FSMC_NORSRAMTimingInitStructure.FSMC_CLKDivision = 0;

      FSMC_NORSRAMTimingInitStructure.FSMC_DataLatency = 0;

      FSMC_NORSRAMTimingInitStructure.FSMC_AccessMode = FSMC_AccessMode_A;

      /* Color LCD configuration ------------------------------------

         LCD configured as follow:

            - Data/Address MUX = Disable

            - Memory Type = SRAM

            - Data Width = 16bit

            - Write Operation = Enable

            - Extended Mode = Enable

            - Asynchronous Wait = Disable */

      FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM1;

      FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable;

      FSMC_NORSRAMInitStructure.FSMC_MemoryType = FSMC_MemoryType_NOR;

      FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b;

      FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable;

      FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable;

      FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;

      FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable;

      FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState;

      FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;

      FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable;

      FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable;

      FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable;

     //FSMC_NORSRAMInitStructure.FSMC_ContinousClock = FMC_CClock_SyncOnly;

      FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &FSMC_NORSRAMTimingInitStructure;

      FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &FSMC_NORSRAMTimingInitStructure;

      FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure);

      /* Enable FMC NOR/SRAM Bank3 */

      FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM1, ENABLE);

    }