Skip to main content
hg-chen
Associate III
April 4, 2007
Question

can not pull the pin stage from low to high when connect 2 ARM together?

  • April 4, 2007
  • 2 replies
  • 606 views
Posted on April 04, 2007 at 09:05

can not pull the pin stage from low to high when connect 2 ARM together?

This topic has been closed for replies.

2 replies

hg-chen
hg-chenAuthor
Associate III
April 4, 2007
Posted on April 04, 2007 at 08:30

1, connect 2 pins of 2 ARM together,

both pins configured as open drain,

with external pull high resistors to 3.3V

2, initila at high state, then pull low by instruction

but can not pull high anymore!

any idea ?

kleshov
Associate
April 4, 2007
Posted on April 04, 2007 at 09:05

If the line stays low, then something is pulling it low. It can be either of the two ARMs. Double-check everything.