Skip to main content
hg-chen
Associate III
November 24, 2006
Question

programming socket board for STR711FR2H6 available?

  • November 24, 2006
  • 4 replies
  • 863 views
Posted on November 24, 2006 at 10:53

programming socket board for STR711FR2H6 available?

This topic has been closed for replies.

4 replies

hg-chen
hg-chenAuthor
Associate III
November 15, 2006
Posted on November 15, 2006 at 23:02

Is the programming socket board for STR711FR2H6(BGA 64) available?

hg-chen
hg-chenAuthor
Associate III
November 20, 2006
Posted on November 21, 2006 at 00:18

or if I want to make a programming socket board myself,

is the AN1775, STR71X HARDWARE DEVELOPMENT GETTING STARTED ,

the file I should refer to for H/W pin connection?

jgoril
Associate III
November 21, 2006
Posted on November 21, 2006 at 07:45

I can offer you the following one:

DIL48/LFBGA64 ZIF STR71x, consists of 2 pieces:

BGA-TOP-84, ord. no. 70-0532 (more info at

http://www.elnec.com/sockcon_info.php?id=BGA-Top-84_ZIF

) and

BGA-BOTTOM-46, ord. no. 70-0531 (more info at

http://www.elnec.com/sockcon_info.php?id=BGA-Bottom-46

)

Certainly, it works only with our universal device programmers that support STR71x devices (Beeprog, BeeHive).

kaouther
Associate II
November 24, 2006
Posted on November 24, 2006 at 10:53

The STR71x Hardware getting started A.N describes the minimum hardware resources required to develop an STR71x application independently of any package type.

Please have a look into the STR71x datasheet and you will find the STR711 BGA Ball Connections.