Skip to main content
ricardof
Associate III
April 1, 2004
Question

Evaluation board, can anyone help me, please ??

  • April 1, 2004
  • 2 replies
  • 575 views
Posted on April 01, 2004 at 21:35

Evaluation board, can anyone help me, please ??

This topic has been closed for replies.

2 replies

joseph2399
Associate II
May 17, 2011
Posted on May 17, 2011 at 11:59

I assume you are using a DK3300 board since the M41ST87 is a Real Time Clock chip (and is on the DK3300 board).

I suspect that you did not define port 1.0 pin function as ''GP I/O mode'' in PSDsoft when you were configuring the device. Go back to PSDsoft and define that pin as such.
ricardof
ricardofAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:59

I´m working with the evaluation board M41ST87 of ST, and I want to text the line P1_0 of the uProcesador, this line is the CPU_ADC0, pin 52, if I want to output in this line one alternaty line, I have programmed the next, and is impossible to see with the osciloscoper the right signel, I don´t kown why ?

P1SFS0 = 0x00; // port 1 of uP, like GPIO

P1_0 = ~P1_0; // change the line constinuosly

In the windows of the pararell port, appears the signal P1_0 changing, but with the osciloscoper in pin 52 is impossible to see it, Why ?