Skip to main content
hpaskal
Associate III
June 18, 2004
Question

bootl and hex file

Posted on June 18, 2004 at 03:07

bootl and hex file

This topic has been closed for replies.

2 replies

hpaskal
hpaskalAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 12:01

I configured my loader project much like the example of the upsd33xx boot.

my loader project psd configuration is like this (i copy it from the .abl file):

rs0 = ((address >= ^h2000) & (address <= ^h3FFF));

csiop = ((address >= ^h0200) & (address <= ^h02FF));

fs0 = ((page == 0) & (address >= ^h8000) & (address <= ^hFFFF));

fs1 = ((page == 1) & (address >= ^h8000) & (address <= ^hFFFF));

fs2 = ((page == 2) & (address >= ^h8000) & (address <= ^hFFFF));

fs3 = ((page == 3) & (address >= ^h8000) & (address <= ^hFFFF));

fs4 = ((page == 4) & (address >= ^h8000) & (address <= ^hFFFF));

fs5 = ((page == 5) & (address >= ^h8000) & (address <= ^hFFFF));

fs6 = ((page == 6) & (address >= ^h8000) & (address <= ^hFFFF));

fs7 = ((page == 7) & (address >= ^h8000) & (address <= ^hFFFF));

csboot0 = ((address >= ^h0000) & (address <= ^h1FFF));

1)My real program is a different uv2 project from the loader project.

My real program uv2 project don't know the configuration of the Loader project.

I have no psd configuration project for my real project .

i have only one psd configuration that i merge with the loader firmware and burn it to the secondary flash with the jtag.

My real program uv2 just output a single *.hex file after he was compiled and linked with keil uv2 tool.

this hex file that i will need to burn in the main flash as my real program ,

only knows that he have xdata from 0x2000 - 0x3FFF.

it is not familiar with the paging that i configured in the loader project .

so , the hex file address fields is incorrect .

so i cant just burn the data in the hex file in the addresses that comes from this file .

How do i manage this ?

thanks

[ This message was edited by: hpaskal on 15-06-2004 15:28 ]
joseph2399
Associate II
May 17, 2011
Posted on May 17, 2011 at 12:01

AN1816 may provide some help. It can be found in the Downloads section for the uPSD products:

http://www.stmcu.com/modules.php?name=mcu&file=familiesdocs&fam=80

[ This message was edited by: uPSD on 18-06-2004 06:40 ]