Skip to main content
raphael23
Associate
April 19, 2004
Question

ST10 272 2nd UART

  • April 19, 2004
  • 5 replies
  • 1268 views
Posted on April 19, 2004 at 10:49

ST10 272 2nd UART

This topic has been closed for replies.

5 replies

raphael23
raphael23Author
Associate
April 9, 2004
Posted on April 09, 2004 at 07:31

Hello,

We are currently using a ST10 269 and began porting/adapting SW to a 272b. We currently use the only available doc, i.e. the 276 one.

Is the new 2nd UART cell the same on 272 as on 276 (same registers) ?

Do you have some sample code to configure the UART (ASC1) ?

Thanks in advance,

Raphael.
charles239955_st
Visitor II
April 9, 2004
Posted on April 09, 2004 at 08:43

Hello,

The 2nd UART is exactly the same in the F272x and the F276. Same registers at same addresses.

It is also the same cell as the UART of the F269 that was ''copied'' and put on the XBus interface. The only difference with the ASC0 is that the registers on the XBus are not bit addressable and do not support byte accesses.

Otherwise the same code that is running on the UART0 will run on the UART1 after changing the name of the registers.

The last ''porting'' action is the interrupt part. You need to use the XIRySEL registers together with the corresponding XPzIC register.

Regards,

Kenshin
raphael23
raphael23Author
Associate
April 9, 2004
Posted on April 09, 2004 at 13:45

Thanks a lot for your quick answer !.

If I've well understood, today I have for instance the following code :

S0PEN = CHECK_PARITY;

S0ODD = EVEN_PARITY;

I've not the right to write

S1PEN = CHECK_PARITY;

S1ODD = EVEN_PARITY;

because the new registers are not bit addressable.

So I should write :

SET.5 = CHECK_PARITY;

CLR.12 = EVEN_PARITY;

Is it right ? It seems strange to me. I don't know if you could provide some example or the reg272.h file that defines all registers name ??

Best regards,

Raphael

najoua
Associate
April 12, 2004
Posted on April 12, 2004 at 08:33

Hello,

You will find in attachment the ''regh'' file. It can be used for ST10F

________________

Attachments :

reg276.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzr2&d=%2Fa%2F0X0000000bY3%2FZWoqclkkItzoHIbMYSmJE8uEkHJ81nhpD9fCo5bICZE&asPdf=false
raphael23
raphael23Author
Associate
April 19, 2004
Posted on April 19, 2004 at 10:49

Thanks a lot.

Raphael.