Skip to main content
shinnlin
Associate III
July 23, 2004
Question

debugging problem

  • July 23, 2004
  • 2 replies
  • 678 views
Posted on July 23, 2004 at 05:12

debugging problem

This topic has been closed for replies.

2 replies

shinnlin
shinnlinAuthor
Associate III
July 21, 2004
Posted on July 21, 2004 at 09:07

I wrote a program as this :

void main(void)

{

int i;

int array[10];

for (i=0; i

array[i] = i+1;

while (1);

}

when I watch the variable 'array' in the while loop,

the displayed data in the watch window is shift, like this:

array [0x2000FA74]

[0] 0x00000002

[1] 0x00000003

[2] 0x00000004

[3] 0x00000005

[4] 0x00000006

[5] 0x00000007

[6] 0x00000008

[7] 0x00000009

[8] 0x0000000A

[9] 0xE59FF018

the value at [0x2000FA70] is 0x00000001

if I look at the dsm code, the start address of 'array' is

[0x2000FA70], not [0x2000FA74].

any one know what's going on with this ?

shinnlin
shinnlinAuthor
Associate III
July 21, 2004