Skip to main content
massimo2399
Associate
May 21, 2004
Question

option byte configuration of ST62T42B

  • May 21, 2004
  • 3 replies
  • 834 views
Posted on May 21, 2004 at 10:06

option byte configuration of ST62T42B

This topic has been closed for replies.

3 replies

massimo2399
Associate
May 19, 2004
Posted on May 19, 2004 at 12:52

hi all!

The 4th bit of the option byte of micro ST62T42B is reserved and it is normally set to 1 by the epromer.

Is it necessary to set to 1 this bit?

bye

max66

vikas2
Visitor II
May 21, 2004
Posted on May 21, 2004 at 02:55

Change in Reserved bits is not recommended and if the reserved bit status is changed, the proper functionality of the device is not guaranteed. So better try not to change their state and maintain the recommended one.

massimo2399
Associate
May 21, 2004
Posted on May 21, 2004 at 10:06

Quote:

On 2004-05-21 06:25, Vikas wrote:

Change in Reserved bits is not recommended and if the reserved bit status is changed, the proper functionality of the device is not guaranteed. So better try not to change their state and maintain the recommended one.

mailto:massimo.bonaiti@rielloboilers.com