Skip to main content
amitb_4
Associate
June 21, 2004
Question

Hive Based Registry for STPC SBC using WinCE

  • June 21, 2004
  • 2 replies
  • 795 views
Posted on June 21, 2004 at 13:44

Hive Based Registry for STPC SBC using WinCE

This topic has been closed for replies.

2 replies

amitb_4
amitb_4Author
Associate
June 2, 2004
Posted on June 02, 2004 at 12:23

I have Developed a platform using WinCE for STPC x86 based SBC. When I change the Storage Registry from RAM based to Hive Based the plateform is not a bootable in SBC. Can anybody tell me about that metter? Is there any change required in the files. I take the tools from that available in WinCE4.2 version.

[ This message was edited by: AmitB on 02-06-2004 15:53 ]
chris_s
Associate II
June 21, 2004
Posted on June 21, 2004 at 13:44

G'day

Check out the platform.reg. Do you have the right things in the hive boot section? As much I remember I had to do just some changes in [HKEY_LOCAL_MACHINE\init\BootVars]. The following stuff shut be in hive boot section:

- [HKEY_LOCAL_MACHINE\init\BootVars]

- [HKEY_LOCAL_MACHINE\Drivers\Resources\IRQ

- [HKEY_LOCAL_MACHINE\Drivers\BuiltIn\PCI]

- #include ''$(DRIVERS_DIR)\block\atapi\ALI1543.reg''

- #include ''$(DRIVERS_DIR)\block\msflashfmd\sdnpci\sdnpcid\sdnpcid.reg''

- [HKEY_LOCAL_MACHINE\Drivers\BuiltIn\Atapi]

Does someone have some experience with putting the system.hv on a Static RAM instead the IDE- Drive? (in WinCE 4.2)

Chris

*** parts of platform.reg ***

; @CESYSGEN IF FILESYS_FSREGHIVE

; HIVE BOOT SECTION

; 2003-07-11: changes

[HKEY_LOCAL_MACHINE\init\BootVars]

''SYSTEMHIVE''=''Documents and Settings\\system.hv''

''PROFILEDIR''=''Documents and Settings''

;''PROFILEDIR''=''Documents and Settings portrait''

''Start DevMgr''=dword:1

''DefaultUser''=''User''

; : end of changes

; END HIVE BOOT SECTION

; @CESYSGEN ENDIF FILESYS_FSREGHIVE

[ This message was edited by: chris_s on 23-06-2004 15:40 ]