Skip to main content
bigsmile
Associate II
February 4, 2005
Question

st7fmc very slow

  • February 4, 2005
  • 6 replies
  • 1121 views
Posted on February 04, 2005 at 09:42

st7fmc very slow

This topic has been closed for replies.

6 replies

bigsmile
bigsmileAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 10:18

hi

first i want to thank you for your help.

i haven't tried to prgramm the multiplication in asm, because i'm not used to programming asm. i only have tried to measure how long the µc takes for several operations and there i found that a multiplication of two 16 bit numbers takes a lot of time.

i don't want to use asm code, because no one will be able to understand the code in a few months or years.

thanks for your help

nice greetings

klaus

gaetano
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:18

Hello,

have you tried to perform such a computation by writing from your own the multiplication operation using ASM coding so avoiding the overload caused by the C compiler?

Regards,

Tanio

bigsmile
bigsmileAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 10:18

hello

my st7fmc takes 31µs to multiplicate two 16bit variables. I'm using the metrowerks compiler. I know that it's difficult for the µC to handle 16bit variables, but this time is impossible for my application. can anyone tell me if this is right or do I have problems with compiler settings or something else.

thanks a lot for your help

best greetings

klaus

gaetano
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:18

Dear Billino,

welcome to the motor control forum dedicated to ST micro products.

Your calculus seems correct, and effectively 15 us seconds are acceptable when multiply to 16 bits operands.

Best regards,

Tanio

stello
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:18

Hi Guys,

sorry for my intrusion...

what is the clock frequency you are using?

If you use 8MHz, 122 cycles are equivalent to about 15usec... It's not too bad..., is it?

luca239955_st
Associate II
May 17, 2011
Posted on May 17, 2011 at 10:18

Hi,

low level routines such as integer multiply are wrtitten in assembler (by the compiler company) anyway.

For example, here is what you get with Cosmic:

; INTEGER MULTIPLY

; Copyright (c) 1998 by COSMIC Software

; - 1st operand in X:A

; - 2nd operand in Y and extension

;

xdef c_imul

xref.b c_y

.dcall ''3,0,c_imul''

;

c_imul:

push a ; save LSB1

ld a,y ; load LSB2

mul x,a ; H * L

ld c_y+1,a ; save in memory

ld x,c_y ; load MSB2

pop a ; load LSB1

push a ; and save it

mul x,a ; L * H

add a,c_y+1 ; accumulate

ld c_y+1,a ; and store

pop a ; load LSB1

ld x,y ; load LSB2

mul x,a ; L * L

push a ; save LSB

ld a,x ; accumulate

add a,c_y+1 ; MSB

ld x,a ; in place

pop a ; restore LSB result

ret ; and return

;

end

this executes in 122 cycles, which, I guess, is consistent with the timing you measured (just multiply by the internal frequency you are using to check).

Conclusion is, there seem to be no solution to your problem.

Hope this helps.

Regards,

Luca

PS: if you think multiplication is slow, don't even try the division...