Skip to main content
phil239955
Associate II
January 21, 2005
Question

STVD7 and Windows XP Pro

  • January 21, 2005
  • 4 replies
  • 963 views
Posted on January 21, 2005 at 14:06

STVD7 and Windows XP Pro

This topic has been closed for replies.

4 replies

phil239955
Associate II
January 19, 2005
Posted on January 19, 2005 at 06:03

We are having problems installing STVD7 on a machine running Windows XP pro. When the installation gets to the stage that it wants to istall the parallel port driver, the system crashes and reboots.

The driver does not appear to get installed and re-running the installer does not fix the problem. We cannot connect to the STICK because the parallel port driver is not installed. This was with the latest version of STVD7 downloaded today.

Does anyone know how to fix this, or how to get the driver installed another way?

sjo
Associate III
January 19, 2005
Posted on January 19, 2005 at 20:24

Only a guess but do you have admin privileges ?

This is required in NT/XP to install any drivers

Regards

sjo

phil239955
Associate II
January 20, 2005
Posted on January 20, 2005 at 04:37

Yes we are definitely installing it with admin privilidges

alain2399
Visitor II
January 21, 2005
Posted on January 21, 2005 at 14:06

Which version of XP is it ?

I suspect SP2 as it is known to bring pbs and also because I have XP SP1 and no pb of install.

Did you install Codewarrior as it may install a old version of the paralel port driver that crashes XP at uninstall.

Alain