My application run for 30 minuts and after...one driver crash (smoke and flash, distructive!!!). Question: I have wrong the parallel connection? I have try also to insert R of 100K and C of 5.6nF between pin microcontroller and driver:
Posted on May 17, 2011 at 10:14Hello, Since the driver gets damaged after some time and not immediately, it looks like to be an effect of high current/temperature. Try using 5.6nF instead of 68nF on EN pins. This should lower the r.m.s. value of the motor (and driver) current during the overload (the maximum r.m.s. current in paralleled configuration is 5.6A and). Overcurrent threshold is at about 11.2A. Care should be taken to avoid electrical overstress of the IC pins (especially SENSE and OUT ones) as well, which might be due to parasitic inductances on pcb traces causing voltage spikes. Please also refer to AN1762 on st.com. Kind regards Vincenzo Marano