Skip to main content
gclink
Associate
May 30, 2005
Question

using ST7 Toolset Devel. tool Visual developer for ST72141 vrs ST72MC.

  • May 30, 2005
  • 2 replies
  • 688 views
Posted on May 30, 2005 at 14:32

using ST7 Toolset Devel. tool Visual developer for ST72141 vrs ST72MC.

This topic has been closed for replies.

2 replies

gclink
gclinkAuthor
Associate
May 17, 2011
Posted on May 17, 2011 at 10:18

Is is possible to convert a project created under the older ST7MTC2 Configuration/Programmer programs ( ie via the *.mtc intermediary file) to the newer ST7 Toolset Devel. tool St7 Visual developer, ie are the old 8 bit assember and linkers there, and can the project files be imported or rebuilt, and if so how?

Also, the excel spread sheet for 8 pole motors is corrupt on my CD, is this file available on your website, and can it generate all the timer values and ration that the Configuration program does ( ie essentially create the mtc file?)

jean-marie
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:18

I send to you the zip file with source and project workspace allowing to assemble soft for ST72141 running on the Kanda kit Hardware. You have to know that this software is running using the SPI communication. Data of the *.mtc file are the one corresponding to dep_prep.txt anddeframp.txt of the project.

I attached a corrected spd82.xls files allowing you to generate the acceleration ramp and to set the speed parameter.