Skip to main content
jeet77_7
Associate
June 6, 2005
Question

facing problem in programming external flash in str710 evaluation board

  • June 6, 2005
  • 6 replies
  • 1340 views
Posted on June 06, 2005 at 09:41

facing problem in programming external flash in str710 evaluation board

This topic has been closed for replies.

6 replies

jeet77_7
jeet77_7Author
Associate
June 4, 2005
Posted on June 04, 2005 at 05:51

Hi every one

i am trying to program a bin file in the external flash in str710 evalution board using realview ice-ME via jtag but not succeding

sequence followed:

1.ttings did on board: Ram boot mode (sw14 at 1-2,sw15 & sw13 at 2-3).

2.Powered on board.

3.Run RVDEBUG software on pc.

4.Clicked ''Connect Target'' and it connected

5.Clicked Debug>memory rigister>upload/download memory

6. filled x.bin file name and memory address (0x60000000)in the dialog appeared.

7.Selected ''load memory from file'' option. in same dilog

8.selected type as ''Raw''

9.Clicked Apply.

10. command appeared at output window but no confirmation or error massage got .

11. then selected option ''varify file'' in same dilog with all settings same.

12. Got error response'' memory missmatch at 0x60000000''

So any help in this regard will be appreciated.

jeetendra

hichem2
Associate
June 6, 2005
Posted on June 06, 2005 at 05:36

Hi jeetendra,

Please can you tell me if you use the last version of the FME files,

if yes be sure that you are connected under ST-STR710-EVAL.

Cheers,

Hich :p

jeet77_7
jeet77_7Author
Associate
June 6, 2005
Posted on June 06, 2005 at 05:40

i got the problem actually there is no fme file for evaluation board external flash and even there is no entry for the external flash in the bcd file .

so i did the entry in bcd file but i still required fme file for the extarnal flash.

jeet77_7
jeet77_7Author
Associate
June 6, 2005
Posted on June 06, 2005 at 06:53

Dear ibtiss

thanks for your response

i already used st710-eval for connection and failed to program external flash.

after that i checked bcd file for st710-eval , in that file there is no entry for the external flash.

i studied an110 of arm and inserted an entry into the bcd file for external flash.

but i need fme file for the external flash used in the board.

best regards

jeetendra

jeet77_7
jeet77_7Author
Associate
June 6, 2005
Posted on June 06, 2005 at 07:45

Dear Ibtiss

the RVDK version is 1.6.1

Regards

Jeetendra

jeet77_7
jeet77_7Author
Associate
June 6, 2005
Posted on June 06, 2005 at 09:41

Thanks ibtiss

loaded successfully

best regards

jeetendra