Skip to main content
xaviooo
Associate III
April 6, 2007
Question

UART - printf on Hyperterminal - STR750 EVAL

  • April 6, 2007
  • 4 replies
  • 842 views
Posted on April 06, 2007 at 13:30

UART - printf on Hyperterminal - STR750 EVAL

This topic has been closed for replies.

4 replies

xaviooo
xavioooAuthor
Associate III
April 6, 2007
Posted on April 06, 2007 at 08:11

Hi,

I'm currently trying to display some messages (necessary to debug a more complex application) on the HyperTerminal of Windows, using an UART.

I'm working with a STR750-EVAL and the Raisonance IDE (with RLINK).

The AN : UM0218 gives a useful example of what i'm trying to do (readme, headers, sources...). (/examples/uart/example 6)

My problem is that this example doesn't work. I get nothing on the Hyperterminal when I call the printf function, although I get something when I use the function Uart_SendData().

The main3.c contains a function fputc who is supposed to retarget the C library printf function to the UART.

Is this example supposed to work ? (with Raisonance IDE, Rlink, and the files I have attached).

Should I re-implement the fputc function in main3.c ?

Should I add something else in the ''.c'' files ?

Thank you in advance.

________________

Attachments :

UART_printf_STR750.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtIh&d=%2Fa%2F0X0000000aLH%2FM13fjexAeH0BZY6VkJHmDXdoWSXZx2iX6jxLdY9Uh_g&asPdf=false
vincentchoplin9
Visitor II
April 6, 2007
Posted on April 06, 2007 at 08:14

Hi,

The printf function will call putchar function in the end. So it is putchar, not fputc, that you need to rewrite.

Or you can use the default UART0_putchar. See this example:

c:\ride\examples\strx\test

Best Regards,

Vincent

vincentchoplin9
Visitor II
April 6, 2007
Posted on April 06, 2007 at 08:18

You will also find some information on the UART0_putchar in this doc:

(in RIDE) ''help''->''PDF''->''STRX-Tools''->''Getting Started STRX''

look in the section about the library options. (section 2.5.1.1, page 14, in the latest version)

Vincent

xaviooo
xavioooAuthor
Associate III
April 6, 2007
Posted on April 06, 2007 at 13:30

Thank you for you answer.

For people who are using this example, use the UART1 although the library is called Uart0... (I lost 2 hours :p)