Skip to main content
vaughan
Associate II
October 27, 2006
Question

Running from internal flash

  • October 27, 2006
  • 3 replies
  • 969 views
Posted on October 27, 2006 at 20:53

Running from internal flash

This topic has been closed for replies.

3 replies

vaughan
vaughanAuthor
Associate II
October 26, 2006
Posted on October 26, 2006 at 20:00

Hi

I have some code that runs ok when load into RAM via the debugger but will not run when loaded into flash. I am using the GNU tool chain to compile with and OpenOCD to program the flash. I have modified my linker file so that the text section resides in flash and the other sections in RAM. When debugging from flash I can see that it is never getting to my main function. I have attached my startup.s and linker files.

What do I need to do to get my code linked from flash and running correctly?

Thanks

Vaughan

________________

Attachments :

hitex_str7_ram.ld : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtJZ&d=%2Fa%2F0X0000000aLU%2FeUlXDageWzhQsKZdr3J3g730dJF2EfJA7zO6tpD8wkk&asPdf=false

startup.s : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtH1&d=%2Fa%2F0X0000000aKz%2FkTvFiTobZeMmAZmubo1xzeQpwt.u34cv_S7QqhAiEhY&asPdf=false
kleshov
Associate
October 27, 2006
Posted on October 27, 2006 at 03:32

If you are able to debug the code in flash, why don't you tell us exactly where it gets stuck?

vaughan
vaughanAuthor
Associate II
October 27, 2006
Posted on October 27, 2006 at 20:53

Hi

Thanks for the reply but figured out what was happening. When converting from elf to bin I forgot an option so the file being programmed was not correct, stopping the code from running.

Cheers

Vaughan