Skip to main content
sarao
Associate II
Aug 25, 2007 10:17 AM UTC
Question

Clearing ENET Interrupts (ENET_ISR)

Posted on August 25, 2007 at 12:17

Clearing ENET Interrupts (ENET_ISR)

This topic has been closed for replies.

2 replies

m_j_butcher
Associate III
May 17, 2011 7:46 AM UTC
Posted on May 17, 2011 at 09:46

Hi

The method looks correct - simply write the bit to be cleared with 1.

However I see no advantage in collecting the serviced interrupt bits and clearing them all at the end of the routine.

Rather than doing

irqToClear |= 0x00000020;

you could simply do

ENET_DMA->ISR = 0x00000020;

Also it may be an idea to use a loop in the routine so that it only exits when all interrupt have been service (an interrupt can arrive while in the IRQ so it can be serviced without having to first quit.

Eg:

while ((ENET_ISR) & ENET_IER) { // while enabled interrupts waiting, handle them all

if (ENET_ISR & TX_CURR_DONE_EN) {

ENET_ISR = TX_CURR_DONE_EN; // reset flag

// etc.

}

if (ENET_ISR & RX_ENTRY_EN) {

ENET_ISR = RX_ENTRY_EN; // reset flag

// etc.

}

// etc....

}

Regards

Mark

http://www.uTasker.com

sarao
saraoAuthor
Associate II
May 17, 2011 7:46 AM UTC
Posted on May 17, 2011 at 09:46

What is the proper way to clear the interrupt bits for the ENET_ISR?

Below is some code snippets. Is this the correct way to handle clearing the interrupt? Is there a better way? Is there something else I should do?

I enable the following interrupts:

 

ENET_DMA->IER = 0x00000000; // clear all bits

 

ENET_DMA->IER |= 0x02000000; // TX_MERR_INT_EN

 

ENET_DMA->IER |= 0x00800000; // TX_DONE_EN

 

ENET_DMA->IER |= 0x00400000; // TX_NEXT_EN

 

ENET_DMA->IER |= 0x00000200; // RX_MERR_INT_EN

 

ENET_DMA->IER |= 0x00000080; // RX_DONE_EN

 

ENET_DMA->IER |= 0x00000040; // RX_NEXT_EN

 

ENET_DMA->IER |= 0x00000020; // PACKET_LOST_EN

 

I enable the ENET interrupt vector

 

VIC_Config( ENET_ITLine, VIC_IRQ, 2 );

 

VIC_ITCmd( ENET_ITLine, ENABLE );

 

My ISR gets called okay:

 

void ENET_IRQHandler(void)

 

{

 

u32 currentState = ENET_DMA->ISR;

 

u32 irqToClear = 0;

 

if ( currentState & 0x00800000 ) // TX_DONE_EN

 

{

 

MUTEX_ENET = 1;

 

irqToClear |= 0x00800000;

 

}

 

 

// TODO: Check for Received packet

 

if ( currentState & 0x00000080 )

 

{

 

MUTEX_ENET_REC = 1;

 

irqToClear |= 0x00000080;

 

 

}

 

// TODO: Check for Errors?

 

 

if ( currentState & 0x00000020 )

 

{

 

irqToClear |= 0x00000020;

 

}

 

 

 

// Clear Interupt: Is this okay?

 

ENET_DMA->ISR = irqToClear; // 0xFFFFFFF

 

 

}