Skip to main content
philip1
Associate III
November 26, 2004
Question

HOLD/HLDA used with ST10F269

  • November 26, 2004
  • 2 replies
  • 611 views
Posted on November 26, 2004 at 12:32

HOLD/HLDA used with ST10F269

This topic has been closed for replies.

2 replies

philip1
philip1Author
Associate III
November 25, 2004
Posted on November 25, 2004 at 12:20

I am planning to use the HOLD/HLDA bus sharing mode on the ST10F269 so that another CPU can write into static RAM on the ST10's bus. The data sheet says that signal line such as CSx, RD, WRL etc. are ''pulled up'' during the HOLD state.

Would this be resistively pulled up so that the external device can drive them low to access the said RAM? if so what sort of value should I expect to have to drive 1k or 10's of k?

Thanks

philip1
philip1Author
Associate III
November 26, 2004
Posted on November 26, 2004 at 12:32

Thanks for the info, What I meant was are they resistors and not totem-pole type drivers, i.e. can an external device pull them low without fighting the ST10's pull-ups.

I think you answered that point

thanks

PhilipJ