Skip to main content
trevor2
Associate
February 18, 2009
Question

STM8A Wakeup from Halt by UART?

  • February 18, 2009
  • 4 replies
  • 1725 views
Posted on February 18, 2009 at 09:09

STM8A Wakeup from Halt by UART?

    This topic has been closed for replies.

    4 replies

    trevor2
    trevor2Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 15:02

    Can the STM8A be woken up from HALT by the UART?

    Is it possible to wake up the STM8A with a pin from the UART Message and then Configure the UART?

    mozra27
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:02

    Hi Bassinux,

    SPI also can wake up the device from Halt

    Regards

    mozra

    bassinux
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:02

    Ciao tutti,

    I, want to add, only I2C and CAN can make exit from halt mode for communication interfaces.

    Bassinux :)

    olga
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 15:02

    Uart's interrupts cannot wake up the device from HALT, anyway, as you already said, it is possible to configure the Uart Rx pin as external interrupt before entering in HALT mode and coming back at UART configuration afer waking up (loosing first byte received).

    Regards,

    Olga

    [ This message was edited by: diamond on 29-01-2009 13:58 ]