Skip to main content
ross2
Associate II
October 29, 2004
Question

In field updates

  • October 29, 2004
  • 5 replies
  • 1307 views
Posted on October 30, 2004 at 01:11

In field updates

This topic has been closed for replies.

5 replies

ross2
ross2Author
Associate II
August 10, 2004
Posted on August 10, 2004 at 06:58

There is talk of the STR71x Flash Programmer to update the flash via UART.

Will the inbuilt boot code also support flash update via USB ?

Some of our customers use our kit connected to Laptops, which no longer have serial ports fitted, so an update in the field would be a problem via a serial port.
shinnlin
Associate III
August 11, 2004
Posted on August 11, 2004 at 15:03

As stated in AN1575, ST7 supports ICP and IAP.

However, ICP is not supported by STR71x, right ?

Therefore, just JTAG programming can be used for mass production to program the blank flash as System Boot Mode is reserved now ?

How can we use RealView ICE for multiple programming in production ?
subscriptions2
Visitor II
August 11, 2004
Posted on August 11, 2004 at 23:35

Quote:

On 2004-08-11 14:32, RISC wrote:

STR71x Flash Programmer to update the flash via UART is reserved. You can not use this feature to update the firmware.

EEK!! You can't program the flash using the serial port! That's a problem. When did this happen?

This is going to make it difficult/impossible for me to use this micro (especially since the competition supports serial ISP).

Robert
from-stmcu
Visitor II
October 20, 2004
Posted on October 20, 2004 at 02:05

I agree - unless you can support some sort of in-system programming with a method other than JTAG, we can't distribute firmware updates to customers via email.

Well, unless this is resolved, everyone will be opting for the Philips LPC21xx (show of hands everyone? ok thats decided!)
subscriptions2
Visitor II
October 29, 2004
Posted on October 30, 2004 at 01:11

New user manual, download still marked as reserved.