Skip to main content
cosmapa
Associate III
October 26, 2007
Question

IAP questions

  • October 26, 2007
  • 2 replies
  • 593 views
Posted on October 26, 2007 at 18:39

IAP questions

    This topic has been closed for replies.

    2 replies

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    Dear cosmapa,

    Here Below some elements of your questions

    1) You can go the ''IAP_AN\binary\template project\'' subdirectory where there is template project for IAR (EWARM) , Raisonance (RIDE) and Keil (RVMDK)

    for the final application you would like to put in Flash starting from 0x8002000 address offset. In EWARM this is configured in File ''lnkarm_flash_offset.xcl''

    // Code memory in FLASH

    -DROMSTART=0x8002000 // :o

    2) The file Format of the Object file is a raw binary ''*.bin'' file without formatting : For EWARM the template project is already configured to output a binary file, for RVMDK there is an utility to translate axf (ARM specific) files to binary and the same for Ride, the subdirectory includes a batch file ''hextobin.bat'' that will do the job.

    3) If using EWARM from IAR (that you have) , you can go to Project->Options

    Then Linker and you can activate the listing, either in the debugger

    window or to have txt or HTML file in your ''List'' subdirectory like

    the picture attached.

    I hope that this helps you. For more details you can refer to EWARM documenation on www.iar.com or installed on your Desktop.

    Regards, STOne-32

    [ This message was edited by: STOne-32 on 26-10-2007 22:12 ]

    cosmapa
    cosmapaAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:16

    I read AN2557 on how to do IAP with the UART. It is quite clear but I have a few questions:

    - How to you define segment boundaries with the IAR tool? The Appnote shows how the set the ApplicationAddress to 0x8002000, but then how do I write my code so that it is actually stored at that address.

    - What is the file format of the object file that gets downloaded? I see a .d79 file in the Exe folder. Can it be used as-is?

    - Finally, where/how can I see the detailed resources (ROM & RAM, address and size) used by my program and its components.

    Thanks