Skip to main content
suranjan
Associate II
December 27, 2004
Question

CAPCOM Reload Register

  • December 27, 2004
  • 2 replies
  • 847 views
Posted on December 27, 2004 at 12:35

CAPCOM Reload Register

This topic has been closed for replies.

2 replies

suranjan
suranjanAuthor
Associate II
December 27, 2004
Posted on December 27, 2004 at 08:05

Hello All,

I have a little confusion about reload register. Say, T7 timer is reloaded with the content of T7REL register when T7 overflows from FFFFh to 0000h.Does the reload register also increase its value synchronously with the timer? Or, it only holds a certain value? If the latter case is true, then is the timer reloaded every time with the same content of reload register?

Thanks

suranjan
suranjanAuthor
Associate II
December 27, 2004
Posted on December 27, 2004 at 11:20

Hi Neila,

Thank you very much. I have one more question. In GPT1, do we have such reload register? My idea is that if I use, for example, core timer T3, and if I assign a value to T3, then at every such assigned value the timer will overflow (or underflow). Am I right?

Thanks