Skip to main content
autodash
Associate
December 7, 2004
Question

st10c167

  • December 7, 2004
  • 2 replies
  • 862 views
Posted on December 07, 2004 at 14:50

st10c167

This topic has been closed for replies.

2 replies

autodash
autodashAuthor
Associate
December 7, 2004
Posted on December 07, 2004 at 13:15

I need to read/write st10c167 eeprom by isp.

but I do not have tools that go for programming.

What tool do I need?

With what programmer can realize rewriting ISP(ICP)?

thx

charles239955_st
Visitor II
December 7, 2004
Posted on December 07, 2004 at 14:50

Are you sure it is the St10C167 you are using?

Because this device have 32K of Masked ROM and therefore can not be re-programmed. The content of the ROM is programmed by STMicroelectronics during diffusion based on a hex file provided by the customer.

Anyway you can read the ROM content using a tool based on the bootstrap loader function (as minimon, see link in other discussion) and do a dump.