Skip to main content
eric4
Associate
January 10, 2005
Question

ST10F269 Flash Read Failure...

  • January 10, 2005
  • 1 reply
  • 628 views
Posted on January 10, 2005 at 08:49

ST10F269 Flash Read Failure...

This topic has been closed for replies.

1 reply

eric4
eric4Author
Associate
January 10, 2005
Posted on January 10, 2005 at 08:49

Morning everyone!

I have a problem with my ST10 flash:

I program unused locations in the chip to 0xFF i.e. same as erased value. A periodic check of the complete flash chip sometimes reads a 0xFF value as 0x7F (this happens on average once every 5 times the memory is checked, but typically is random).

Is it possible that when programming an already erased location to 0xFF, that there can be a smaller charge applied holding the state of the flash 'bit' than if I program the value with, e.g. 0x00?

And could this explain why I sometimes read a 0x7F when I should be reading 0xFF?

Thanks all,

Eric Watson

:-[