Skip to main content
lseletron
Associate III
September 13, 2007
Question

RLink connection

  • September 13, 2007
  • 1 reply
  • 644 views
Posted on September 13, 2007 at 04:40

RLink connection

This topic has been closed for replies.

1 reply

lseletron
lseletronAuthor
Associate III
September 13, 2007
Posted on September 13, 2007 at 04:40

Hi,

I am using RLink and ST72F264G2.

I can program the chip, read option byte etc., but I cannot use it to debug.

When I press (in STVD7)the ''Start Debugging'' button it asks me to reduce the sector size to 0.5K and after that it says ''Chip not responding after user reset: check power supply and clock source options''.

There is power and I try with both option byte enabled and disabled, to no avail.

Thank you