Skip to main content
lseletron
Associate III
November 3, 2007
Question

CPU power consumption

  • November 3, 2007
  • 2 replies
  • 853 views
Posted on November 03, 2007 at 17:12

CPU power consumption

This topic has been closed for replies.

2 replies

lseletron
lseletronAuthor
Associate III
September 27, 2007
Posted on September 27, 2007 at 05:54

Hi,

I am using ST72F264G2 powered with 3.3VDC. To lower consumption I put it to Wait mode (cant use Active Halt as I need to receive signals form outside and external interrupt wont wake it up from Active Halt).

My consumption is about 7.3 mA

What would be the power consumption (a guesstimate) if I used ST72F324LK2 which is a chip specially designed for low-power applications.

Will it lower power consumption significantly?

Thank you

patm4
Associate II
November 3, 2007
Posted on November 03, 2007 at 17:12

I know nothing about the ST72F264G2.

However I know the basics of cmos technology. To save power either reduce VDD or fcpu or both.

I use the 72F324J6T6 part at 5v and the IDD is approx 2mA @ 3.6868Mhz xtal freq.

If you are bothered about power always use the lowest xtal freq and VDD you can in your application.

PS I think the B version of the 72F32X/L parts have the wake up on external interrupt feature fixed.