Skip to main content
charly_m2
Associate
August 4, 2005
Question

ST10F269 problem with CAN

  • August 4, 2005
  • 2 replies
  • 795 views
Posted on August 04, 2005 at 07:56

ST10F269 problem with CAN

This topic has been closed for replies.

2 replies

charly_m2
charly_m2Author
Associate
August 4, 2005
Posted on August 04, 2005 at 06:16

Hi,

I am working on an project with ST10F269, using Tasking V7.5 r2.

The program (about 540kB) is stored in an external 1MB flash an working fine. Now I want to add a CAN-connection in order to exchange data with other devices of the same project. But when I enable CAN1 in XPERCON, the program crashes, it seems as if there is any conflict in adressing the external flash.

Does anybody have a hint to solve this problem?

charly_m2
charly_m2Author
Associate
August 4, 2005
Posted on August 04, 2005 at 07:56

Thank you for your answer,

SALSEL is set to 00, and adress-lines > A19 are not used.

So this does not seem to be the problem.