Skip to main content
alandras
Associate III
March 26, 2007
Question

WSR_AHB: AHB Wait state enable ???

  • March 26, 2007
  • 1 reply
  • 685 views
Posted on March 26, 2007 at 11:26

WSR_AHB: AHB Wait state enable ???

This topic has been closed for replies.

1 reply

alandras
alandrasAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:40

If I don't set the WSR_AHB bit in SCR0, memory to memory DMA never finish! (it never starts)

WSR_AHB: AHB Wait state enable

This bit is set and cleared by software to enable/disable the insertion of a wait

state during an SRAM read access performed on the AHB bus

0: No wait state

1: 1 wait state (default)

Like the SRAM arbiter don't let the DMA to access the AHB!

Is this a normal behavior? I'm runing at 96 MHz.

What should I read to understand how these setting influence system performance? Less wait-states should be better ?

WSR_AHB,WSR_DTCM are set by default and usually startup files leave them in 1. It may because of this?

thanks,

Andras