Skip to main content
fabrice23
Associate III
July 5, 2007
Question

Flashing STR750 with RVDK

  • July 5, 2007
  • 3 replies
  • 1009 views
Posted on July 05, 2007 at 07:34

Flashing STR750 with RVDK

This topic has been closed for replies.

3 replies

fabrice23
fabrice23Author
Associate III
April 10, 2007
Posted on April 10, 2007 at 04:18

I'm using RVDK with a STR750 evaluation board from ST.

But I cannot flash a program into Embedded flash memory.

In the window in RVDK,

It displays

Flash Log:

Loading Flash routine...

Initializing Flash routine...

RVDK stucks and never starts to flash.

I already posted this problem, but no right answer yet.

fabrice23
fabrice23Author
Associate III
April 24, 2007
Posted on April 25, 2007 at 01:46

Hello Ibtissem,

First, I'd like to thank you for your reply.

Recently I got another patch from ST Korea, I attach it.

But this patch works only small simple file,

when I tried an example from ST750 standard SW library, i.e., UART-example2, I found no error during flashing into the embedded flash memory,

but it doesn't work to communicate with the hypreterminal.

The BCD file is very small compared to the one from the ST web site.

Could you suggest which one should I use?

Many lines are missing in the str750_mini.bcd (attached one).

Best Wishes,

Byung-Tae Jung

________________

Attachments :

RVDK_v2.1.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtEY&d=%2Fa%2F0X0000000aKb%2FOyMERa8ulIG7dg7DI8vg7mTdpdcrAoS9wO.sX_Tacpk&asPdf=false
fabrice23
fabrice23Author
Associate III
April 25, 2007
Posted on April 25, 2007 at 05:07

Hello Ibtissem,

Here is the test result of your new flash_str750fx2.fme

In short, it caused a Fatal Error.

Best Wishes,

Byung-Tae Jung

________________

Attachments :

fatal_error.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtEi&d=%2Fa%2F0X0000000aKc%2FMZezX0GXTxmar1BixxBQK1BbVbSOLGb6XHpdEbmH558&asPdf=false