Skip to main content
16-32micros
Associate III
September 26, 2008
Question

Welcome ! “STM32 Releasing your Creativity�

  • September 26, 2008
  • 17 replies
  • 2190 views
Posted on September 26, 2008 at 18:23

Welcome ! “STM32 Releasing your Creativity�

    This topic has been closed for replies.

    17 replies

    shangdawei1
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    Welcome to discussions on The New “STM32� microcontroller family from STMicroelectronics !

    Any info about STM32 ?

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    Welcome to discussions on The New “STM32�? microcontroller family from STMicroelectronics.

    Built around the most recent and efficient 32-bit Cortex-M3 Core from ARM™,

    STM32 delivers the computation power you ever dreamed of, while allowing very low power modes and packaged with our ultimate selection of Analogue and Digital peripherals.

    Don't forget to register and login before you start a thread or reply to a message.

    STOne-32 ;)

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    Hi,

    The STM32 family benefits from the Cortex-M3’s many new architectural enhancements including the Thumb-2 instruction set to deliver improved performance combined with better code density, and a tightly-coupled Nested Vectored Interrupt Controller for significantly faster response to interrupts.

    Thumb-2 instruction set provides 32bit performance with 16bit code density,

    gives complete Thumb Compatibility and is a Single POWERFULL instruction set with No more switching between ARM/Thumb modes.

    The most important difference between the Thumb ISA and the ARM ISA is that most 32-bit Thumb instructions are unconditional, whereas almost all ARM instructions can be conditional. However, Thumb-2 introduces a new If-Then (IT) instruction that delivers much of the functionality of the condition field in ARM instructions.

    In addition to the new 32-bit Thumb instructions, there are several new 16-bit Thumb instructions. Several new 32-bit ARM instructions are introduced at the same time.

    For more details you can refer to :

    http://www.arm.com/products/CPUs/archi-thumb2.html

    With best regards,

    STOne-32

    [ This message was edited by: STOne-32 on 11-06-2007 18:59 ]

    m3allem
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    Hello,

    I've heard a lot about Cortex-M3 recently.

    What is the difference between Cortex-M3 and ARM7/9 Thumb and ARM instruction Sets?

    Thanks :)

    [ This message was edited by: M3allem on 11-06-2007 16:01 ]

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    Dear all,

    Here you go :

    http://www.st.com/stm32

    Enjoy discovering the family features :p

    Best Regards,

    STOne-32

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    Hi hild,

    You can find a detailed description about the THUMB2 instruction set in the document ''ARM v7-M Architecture Application Level Reference Manual (beta release)'' available in the following link:

    http://www.arm.com/documentation/Instruction_Set/index.html

    Note: you will be asked to do a registration to download the document.

    With best regards

    STone-32

    hild
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    Is there a single PDF somewhere, which describes

    all Thumb2 instructions of the Cortex-M3 in detail?

    Even on the ARM website I had no luck, just white

    papers which describe some aspects, but not a concentrated

    instruction set of the Cortex.

    i239955_stm1
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    Hello,

    are free samples available? I tried to purchase some, but I have found ST7 only.

    Regards

    Igor

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    Hi hild,

    To order the STM3210B-EVAL board, please contact your local ST distributor.

    With best regards

    STOne-32

    hild
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    hi again,

    thank you for the link. the pdf was very helpful.

    next question: where and when will the eval-boards

    be available? I was checking out all German distributors,

    but they don't even have a clue or awareness of STM3210B-EVAL.

    do you have any information on

    - pricing

    - availability

    how does the STM3210B-EVAL differ from STM3210B-MCKIT and

    STM3210B-PRIMER ?

    thanks again!

    hild.