Skip to main content
16-32micros
Associate III
January 5, 2008
Question

Happy New Year 2008 with STM32 !

  • January 5, 2008
  • 4 replies
  • 865 views
Posted on January 05, 2008 at 19:45

Happy New Year 2008 with STM32 !

    This topic has been closed for replies.

    4 replies

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    Dear all,

    STMicroelectronics, and all STM32 families Team wish you a happy new Year 2008 with plenty of health and success.

    In 2008, STM32 family lines will grow and will see an expansion of the current options with Larger packages up to 512KB Flash, 64KB SRAM and with extended features such as External Memories/Bus support, SDIO, I2S, and DAC with additional features and many new services for our customers.

    All the best for 2008 with STM32 ;)

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    Dear Danielya, Magigimix,

    We appreciate all of your interest and comments about our future microcontrollers. As this kind of information has a sensitive nature,

    we may not respond to this public posts in this forum. The best way to serve you is :

    1)Use our online support structure at

    http://www.st.com/stonline/domains/support/contact_mcu_support.htm

    2)Contact your nearest ST office, our design consultants will provide you

    the details of your inquiries.

    Kind Regards, STOne-32 :o

    asterix
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    Dear STOne-32,

    Another question, does the the External memory Interface is compatible with Nor and Nand flash ? I would like to use both in my scanner application one for code and the other for data logging. Thank You.

    Magigimix

    [ This message was edited by: asterix.magigimix on 01-01-2008 22:46 ]

    danielya
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    Dear STOne-32

    I am going to use this year the STM32 in several projects, but most

    important is the laser beam position sensor for the monitoring

    of large experimental setups in CERN accellerator experiments.

    The only feature which I need in addition to the STM32F103 series

    existing chips is DAC. Concerning I want to ask.

    1. If it is planed to have DAC in small package 36 and/or 48 pin?

    2. If yes, then when approximatelly I can expect to have samples?

    Thank you in advance,

    Varuzhan