Skip to main content
rwojtanowski
Associate
June 14, 2007
Question

What is differences between L6235 and L6229 (driver for 3-phase BLDC motor)

  • June 14, 2007
  • 2 replies
  • 830 views
Posted on June 14, 2007 at 09:46

What is differences between L6235 and L6229 (driver for 3-phase BLDC motor)

This topic has been closed for replies.

2 replies

vincenzo1
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:14

The only difference is the size of integrated power mosfets (i.e. maximum current). Choosing between L6235 and L6229 and the package type (SO, PowerDIP, PowerSO) take into account power dissipation more than rated current (see datasheet and app.notes).

Regards

Vincenzo MARANO

STMicroelectronics

rwojtanowski
Associate
May 17, 2011
Posted on May 17, 2011 at 10:14

What is differences between L6235 and L6229 (driver for 3-phase BLDC motor) - only output current ?

I want to drive 3-phase bldc motor ( 1A max output current, 120° Hall efect decoding logic) - It really doesn't mater which chip I will use ?