Skip to main content
adrian3
Associate II
August 20, 2007
Question

Fault Tolerant I/O

Posted on August 20, 2007 at 05:54

Fault Tolerant I/O

    This topic has been closed for replies.

    2 replies

    anis2399
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    Hi _adrian_,

    - The 5V tolerant (FT) refers to the input level for the pins... the STM32 pins with FT capability can support 5V as input but can't generate 5V.

    - The best way to use the PB5 as FT is to add an external level translator...

    Regards

    The Lionheart

    adrian3
    adrian3Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:15

    In the pin descriptions section of the data sheet (Table 3), each pin is defined as whether it is 5V tolerant (FT). Unfortunately, PB5 (which I hope to use as an open drain output - returned to 5V) is not shown as being FT.

    Q. Does the term 'FT' refer to the input or the output function - or both?

    Q. What would be the best way to ensure this pin is FT?

    I was thinking along the lines of an N channel FET as per Figure 20 in the UM0426 Evaluation board User Manual

    Any thoughts?

    [ This message was edited by: _adrian_ on 25-07-2007 11:47 ]