there are 5 examples for I2C : Example1 : Transfer a data buffer from I2C1 to I2C2 using interrupts. Example2 : Transfer two data buffer from I2C1 to I2C2 through its two addresses in the same application. Example3 : Send an ARP command from I2C1 to I2C2 in SMBus mode. Example4 : Transfer a data buffer from I2C1 to I2C2 in 10-bit addressing mode.. Example5 : Use the I2C firmware library and an associate I2C EEPROM driver to communicate with an M24C08 EEPROM. Regards, STOne-32. [ This message was edited by: STOne-32 on 12-10-2007 22:24 ]
I am using a STM32F103 and trying to write (interrupt driven) code for a slave transmitter. (slave receiver works fine). I get the I2C_EVENT_SLAVE_TRANSMITTER_ADDRESS_MATCHED event in the ISR, and read I2C_GetLastEvent (reads SR1, SR2 to clear ADDR), and TXE is 1 before I send data. When I try to send data, I dont see anything on the master. Am I missing anything?
Do you have any sample code fo the I2c slave in Tx mode /combined (Rx to Tx) mode ? Any help will be greatly appreciated.
The I2C_EVENT_SLAVE_BYTE_TRANSMITTED event requires the BTF bit to be asserted. This never occurred in my case. I worked with one of the ST app engineers on this but I've not gotten a response back yet. An easy fix for me was to generate a new event which excludes the BTF and that seems to work fine. Regards, skeating
Have you been able to resolve the problem? I'm currently in the same situation. I have taken Example 1 of the ST sample code and attempted to re-write it to perform a basic Master receiver (I2C1) - Slave transmitter (I2C2) but have been unsuccessful at this point. I too see the I2C_EVENT_SLAVE_TRANSMITTER_ADDRESS_MATCHED occur but I never get to the I2C_EVENT_SLAVE_BYTE_TRANSMITTED event. Regards, skeating