Skip to main content
tibo
Associate II
June 13, 2008
Question

emulator with trace

  • June 13, 2008
  • 2 replies
  • 780 views
Posted on June 13, 2008 at 17:51

emulator with trace

    This topic has been closed for replies.

    2 replies

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:37

    Dear Tibo,

    Thank for your detailed request. Me too I have an JTAGJetTrace working with STR9 but not yet for STM32 High-density devices that supports trace/ETM. I will note your point and check my colleagues if we can negociate with Signum to provide this service and a full package with STM32.

    However I can suggest you to check with Segger in germany at www.segger.com :

    http://www.segger.com/jtrace_general.html

    (Less than 1000Euros) , I believe that they are already working on STM32.

    I can also advice you to use Serial Wire Viewer for extreme low-cost solution but with limited features at :

    http://www.st.com/mcu/contentid-115.html

    Hope this is us useful for you :)

    Cheers,

    STOne-32 ... Welcome to our recently 8-bit STM8S Family too :)

    tibo
    tiboAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:37

    Hi ST1,

    we are searching for a trace emulator for the stm32. I think Signum

    has a good trace emulator with stm32 support (with ITM and ETM), but

    it was very expensive for a ''low cost'' chip like stm32.

    I found on the homepage of Signum an ARM Evaluation Kit ''JTAGjet-

    Trace-STM''. The price is $2.500,- (normal price > $3.500,-). So I

    asked Signum, if it can be used with stm32. Here is the answer:

    > This was a special OEM version of JTAGjet-Trace which was

    > designed for ST. ST commissioned Raisonance to supply a

    > complete solution for STR9 including our JTAGjet-Trace. So we

    > built them a special firmware inside to limit its operation to STR9

    > devices only and sold it for $2,500.

    >

    > This item is only available from ST or its distributors.

    Now my question to ST is, if it is possible to make this trace

    emulator available for the stm32-community. I think it is only a

    question of licensing and not of hardware/software, because Signum

    supports already the stm32.

    Thanks!