Skip to main content
John F.
Associate III
June 28, 2012
Question

STM32F4 TIM1 PWM missing ch1..3

Posted on June 28, 2012 at 17:48

STM32F4 TIMER 1 PWM1. Please can someone tell me how to enable channels 1, 2 and 3. Channel 4 is fine generating a PWM at 0..100% at 20Hz. I know channels 1..3 hardware is different - just can't figure out what to do to get the outputs enabled.

Thanks.

#include ''stm32f4xx.h'' //CMSIS Cortex-M4 Device Peripheral Access Layer Header File.
#include ''main.h''
uint16_t CCR1_Val = 30; //LED PWM range 0..100
uint16_t CCR2_Val = 40;
uint16_t CCR3_Val = 50;
uint16_t CCR4_Val = 60;
int main (void)
{
/*
At this stage the microcontroller clock setting is already configured by the 
SystemInit() function called from startup file (startup_stm32f4xx.s). To reconfigure 
the default setting of SystemInit() function, refer to system_stm32f4xx.c file. 
*/
//enable peripheral clocks before attempting to initialise them
//for PWM based on Timer1 using GPIO on port E
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE);
//initialise the NVIC before configuring or enabling peripherals
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4); //4 bits for pre-emption priority 0 bits for subpriority
//initialise the GPIO and alternate functions to set up hardware
GPIO_Configuration_PWM();
//finally, initialise peripherals as required
Timer1_Configuration();
while(1); // Spin endlessly
}
void GPIO_Configuration_PWM(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* GPIOE Configuration: TIM1 CH1 (PE9), TIM1 CH2 (PE11), TIM1 CH3 (PE13) and TIM1 CH4 (PE14) */
GPIO_InitStructure.GPIO_Pin = (GPIO_Pin_9 | GPIO_Pin_11 | GPIO_Pin_13 | GPIO_Pin_14);
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
GPIO_Init(GPIOE, &GPIO_InitStructure);
// Connect TIM1 pins to AF
GPIO_PinAFConfig(GPIOE, GPIO_PinSource9, GPIO_AF_TIM1);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource11, GPIO_AF_TIM1);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource13, GPIO_AF_TIM1);
GPIO_PinAFConfig(GPIOE, GPIO_PinSource14, GPIO_AF_TIM1);
}
void Timer1_Configuration(void)
{
//timer 1 is clocked by APB2 at 84MHz, prescale by 42000 to get 2kHz clock
//use a period of 100 cycles to get 0..100% granularity and 20Hz frequency
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);
TIM_TimeBaseStructure.TIM_Period = (100-1);
TIM_TimeBaseStructure.TIM_Prescaler = (42000-1);
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
/* PWM1 Mode configuration: Channel1 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; 
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR1_Val;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM1, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Enable);
/* PWM1 Mode configuration: Channel2 */
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR2_Val;
TIM_OC2Init(TIM1, &TIM_OCInitStructure);
TIM_OC2PreloadConfig(TIM1, TIM_OCPreload_Enable);
/* PWM1 Mode configuration: Channel3 */
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR3_Val;
TIM_OC3Init(TIM1, &TIM_OCInitStructure);
TIM_OC3PreloadConfig(TIM1, TIM_OCPreload_Enable);
/* PWM1 Mode configuration: Channel4 */
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR4_Val;
TIM_OC4Init(TIM1, &TIM_OCInitStructure);
TIM_OC4PreloadConfig(TIM1, TIM_OCPreload_Enable);
TIM_ARRPreloadConfig(TIM1, ENABLE);
//required for timers 1 or 8
TIM_CtrlPWMOutputs(TIM1, ENABLE);
/* TIM1 enable counter */
TIM_Cmd(TIM1, ENABLE);
}

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    June 28, 2012
    Posted on June 28, 2012 at 18:18

    Use TIM_OCStructInit() to clear out the other four settings to meaningful values, not stack junk.

      TIM_OCInitStruct->TIM_OutputNState = TIM_OutputNState_Disable;

      TIM_OCInitStruct->TIM_OCNPolarity = TIM_OCPolarity_High;

      TIM_OCInitStruct->TIM_OCIdleState = TIM_OCIdleState_Reset;

      TIM_OCInitStruct->TIM_OCNIdleState = TIM_OCNIdleState_Reset;

    Other than that the code looks like it should work.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    John F.
    John F.Author
    Associate III
    June 28, 2012
    Posted on June 28, 2012 at 21:22

    Thanks, I'll try that tomorrow and report back.

    John F.
    John F.Author
    Associate III
    June 29, 2012
    Posted on June 29, 2012 at 09:10

    That fixed it! Thanks. Added structure initialisation ...

    TIM_OCStructInit(&TIM_OCInitStructure); //added THIS
    /* PWM1 Mode configuration: Channel1 */