Skip to main content
passafabio2
Associate II
November 3, 2016
Question

Old discovery stm32F407 with chip rev. A, I2C issue

  • November 3, 2016
  • 3 replies
  • 829 views
Posted on November 03, 2016 at 17:18

I tried a lot of time generate I2C code with cube MX and AC6 IDE, but I never see SDA or SCL move. I generated code for other I2C than I2C1 but with no success.

Is there any issue using stm32f407VGT6 Rev. A mounted on my Discovery board?

Driving PB6 and PB7 as GPIO in output  mode I see the pin goes high and low...
    This topic has been closed for replies.

    3 replies

    slimen
    Visitor II
    November 3, 2016
    Posted on November 03, 2016 at 18:14

    Hello,

    You can check if this is related to the I2C

    http://www.st.com/content/ccc/resource/technical/document/errata_sheet/0a/98/58/84/86/b6/47/a2/DM00037591.pdf/files/DM00037591.pdf/jcr:content/translations/en.DM00037591.pdf

    :

    Both SDA and SCL maximum rise time (tr) violated when VDD_I2C bushigher than ((VDD+0.3) / 0.7) V

    Regards

    passafabio2
    Associate II
    November 3, 2016
    Posted on November 03, 2016 at 18:43

    Connect to I2C there is an humidity sensor HTU210. The sensor is connected to 3v3 comes from discovery. The voltage measured is 2,98V.

    Also two 4k7 pull up resistor tied the SDA, SCL high.

    Thanks for reply

    Fabio

    passafabio2
    Associate II
    November 3, 2016
    Posted on November 03, 2016 at 18:59

    This is the code generated by CubeMX

    /* Includes ------------------------------------------------------------------*/
    #include ''main.h''
    #include ''stm32f4xx_hal.h''
    /* USER CODE BEGIN Includes */
    /* USER CODE END Includes */
    /* Private variables ---------------------------------------------------------*/
    I2C_HandleTypeDef hi2c1;
    /* USER CODE BEGIN PV */
    /* Private variables ---------------------------------------------------------*/
    #define SIZEI2C_TX 1
    #define SIZEI2C_RX 3
    uint8_t prova1[SIZEI2C_TX]= {0xE3};
    uint8_t prova2[SIZEI2C_RX];
    /* USER CODE END PV */
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    void Error_Handler(void);
    static void MX_GPIO_Init(void);
    static void MX_I2C1_Init(void);
    /* USER CODE BEGIN PFP */
    /* Private function prototypes -----------------------------------------------*/
    /* USER CODE END PFP */
    /* USER CODE BEGIN 0 */
    /* USER CODE END 0 */
    int main(void)
    {
    /* USER CODE BEGIN 1 */
    /* USER CODE END 1 */
    /* MCU Configuration----------------------------------------------------------*/
    /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
    HAL_Init();
    /* Configure the system clock */
    SystemClock_Config();
    /* Initialize all configured peripherals */
    MX_GPIO_Init();
    MX_I2C1_Init();
    /* USER CODE BEGIN 2 */
    HAL_I2C_Master_Transmit (I2C1, (uint8_t )0x40, prova1[0], SIZEI2C_TX, 50);
    /* USER CODE END 2 */
    /* Infinite loop */
    /* USER CODE BEGIN WHILE */
    while (1)
    {
    /* USER CODE END WHILE */
    /* USER CODE BEGIN 3 */
    }
    /* USER CODE END 3 */
    }
    /** System Clock Configuration
    */
    void SystemClock_Config(void)
    {
    RCC_OscInitTypeDef RCC_OscInitStruct;
    RCC_ClkInitTypeDef RCC_ClkInitStruct;
    /**Configure the main internal regulator output voltage 
    */
    __HAL_RCC_PWR_CLK_ENABLE();
    __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
    /**Initializes the CPU, AHB and APB busses clocks 
    */
    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
    RCC_OscInitStruct.HSEState = RCC_HSE_ON;
    RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
    RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
    RCC_OscInitStruct.PLL.PLLM = 8;
    RCC_OscInitStruct.PLL.PLLN = 168;
    RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
    RCC_OscInitStruct.PLL.PLLQ = 4;
    if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
    {
    Error_Handler();
    }
    /**Initializes the CPU, AHB and APB busses clocks 
    */
    RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
    |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
    RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
    RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
    RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
    RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
    {
    Error_Handler();
    }
    /**Configure the Systick interrupt time 
    */
    HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
    /**Configure the Systick 
    */
    HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
    /* SysTick_IRQn interrupt configuration */
    HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
    }
    /* I2C1 init function */
    static void MX_I2C1_Init(void)
    {
    hi2c1.Instance = I2C1;
    hi2c1.Init.ClockSpeed = 100000;
    hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
    hi2c1.Init.OwnAddress1 = 0;
    hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
    hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
    hi2c1.Init.OwnAddress2 = 0;
    hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
    hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
    if (HAL_I2C_Init(&hi2c1) != HAL_OK)
    {
    Error_Handler();
    }
    }
    /** Configure pins as 
    * Analog 
    * Input 
    * Output
    * EVENT_OUT
    * EXTI
    */
    static void MX_GPIO_Init(void)
    {
    GPIO_InitTypeDef GPIO_InitStruct;
    /* GPIO Ports Clock Enable */
    __HAL_RCC_GPIOC_CLK_ENABLE();
    __HAL_RCC_GPIOH_CLK_ENABLE();
    __HAL_RCC_GPIOD_CLK_ENABLE();
    __HAL_RCC_GPIOB_CLK_ENABLE();
    /*Configure GPIO pin Output Level */
    HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);
    /*Configure GPIO pin : PD15 */
    GPIO_InitStruct.Pin = GPIO_PIN_15;
    GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
    }
    /* USER CODE BEGIN 4 */
    /* USER CODE END 4 */
    /**
    * @brief This function is executed in case of error occurrence.
    * @param None
    * @retval None
    */
    void Error_Handler(void)
    {
    /* USER CODE BEGIN Error_Handler */
    /* User can add his own implementation to report the HAL error return state */
    while(1) 
    {
    }
    /* USER CODE END Error_Handler */ 
    }
    #ifdef USE_FULL_ASSERT
    /**
    * @brief Reports the name of the source file and the source line number
    * where the assert_param error has occurred.
    * @param file: pointer to the source file name
    * @param line: assert_param error line source number
    * @retval None
    */
    void assert_failed(uint8_t* file, uint32_t line)
    {
    /* USER CODE BEGIN 6 */
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    /* USER CODE END 6 */
    }