Skip to main content
John F.
Associate III
July 14, 2015
Question

STM32CUBEMX 4.9.0 Updater check fails during access to HTTP Server

Posted on July 14, 2015 at 10:18

I have installed STM32CUBEMX 4.9.0. on my Win7 PC. Using Help/Install New Libraries I can download and install for example Firmware Package for Family STM32F4. However, Help/Check for Updates (or the Check button in the New Libraries Manager pane) produces an error with the Connection to HTTP Server green progress bar stopped at about 50% and the pop up message ''Error during Access to HTTP Server. Please check Proxy ...''

I am using the Use System Proxy Parameters setting but have also tried a manual configuration that works OK with Rowley CrossWorks IDE. Pressing the Check connection button always brings up a green tick regardless of the Proxy Server Type radio button setting.

Is this a CubeMX problem? Any advice please?
    This topic has been closed for replies.

    5 replies

    chrif
    Visitor II
    July 14, 2015
    Posted on July 14, 2015 at 12:03

    Hi John,

    I have installed the cubeMx 4.9.0 and I have updated many packages with no problem.

    Do you use credential sharing? I suspect that the problem is related to your proxy settings.

    Best regards

    John F.
    John F.Author
    Associate III
    July 14, 2015
    Posted on July 14, 2015 at 12:21

    Hi thanks for your response. I work in a secure commercial environment so it's likely the problem is at our end. I just wanted to enquire here first before getting our IT department involved. As I said, the file download works fine but the update check doesn't. I wondered why one part worked when the other doesn't.

    stm32cube-t
    ST Employee
    July 15, 2015
    Posted on July 15, 2015 at 16:54

    Hello John,

    Your issue has not been reproduced.

    Do you still encounter the error?

    Thanks for your feedback.

    John F.
    John F.Author
    Associate III
    July 15, 2015
    Posted on July 15, 2015 at 17:22

    Hi,

    Thanks for following this up. Today - it works. I am using the Use System Proxy Parameters setting and have made no changes. The PC has been powered down overnight and up again this morning. I can't explain it but for now anyway both ''Check for Updates'' and ''Install New Libraries'' are working!

    stm32cube-t
    ST Employee
    July 17, 2015
    Posted on July 17, 2015 at 15:00

    Good news.

    Thank you John for the feedback.