Skip to main content
raptorhal2
Lead
October 18, 2011
Question

ST-One: STM32F4xx ADC Channels

  • October 18, 2011
  • 1 reply
  • 463 views
Posted on October 18, 2011 at 03:34

The data sheet for the STM32F4 series states that 24 external ADC input channels are available, but I can find only 23 in the pin assignments. ADC3_IN8 appears to be missing.

The F4 reference manual (RM0090) describes just 16 external channels.

Please reply with the pin assignment for ADC3_IN8 and, of course, poke your ST brethren to fix the documentation.

Cheers, Hal

    This topic has been closed for replies.

    1 reply

    Nickname12657_O
    Associate III
    October 18, 2011
    Posted on October 18, 2011 at 16:32

    Hi Hal,

    There are 24 ADC input channel for STM32F4: ADC3_IN8 is mapped on PF10 pin.

    Datasheet and RM will be updated.

    Cheers,

    STOne-32.