Question
STM42F4 Pin 1 Identifier
Posted on July 02, 2014 at 02:49
Just received some STM32F405RGT6 (64 pin LQFP) processors with two round circles on opposite corners of the package, one smaller with a concave bottom, the other larger with a flat bottom. The package description in the datasheet of course shows only one mark. Can anyone tell me which is the real Pin 1 identifier ? I suspect it is the smaller circle, but I don't want to risk letting all the smoke out of the chip finding out.
The F405 144 pin LQFP processors also just received correctly have only one pin marker. Thanks, Hal