Skip to main content
ams2
Associate II
February 23, 2010
Question

STM32 with Ethernet and FSMC?

  • February 23, 2010
  • 1 reply
  • 496 views
Posted on February 23, 2010 at 18:14

STM32 with Ethernet and FSMC?

    This topic has been closed for replies.

    1 reply

    gahelton1
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:41

    Is ST still woking on the new STM32 with 90nm?

      YES.

    Will it have FSMC and Ethernet?  It would be great if it did.

    What will be the CPU speed?  Shrinking the geometry almost always will allow an increase in speed along with more memory. How much faster - we will have to wait and see. I would expect a significant speed increase.

    If I were me, I'd be excited !

    http://www.eetimes.com/news/latest/showArticle.jhtml?articleID=220700360

    http://embeddedsystemnews.com/stmicroelectronics-announces-industry’s-first-devices-featuring-embedded-flash-at-90nm-process-technology-based-on-arm-cortex-m-series.html