Skip to main content
ramadevi
Associate II
February 4, 2010
Question

System Bootloader for STM32F107xx

  • February 4, 2010
  • 16 replies
  • 4237 views
Posted on February 04, 2010 at 11:15

System Bootloader for STM32F107xx

#dfuse-v3.0.0 #stm32 #stm32-usb-flash-update #bootloader
This topic has been closed for replies.

16 replies

aleksey
Visitor II
May 17, 2011
Posted on May 17, 2011 at 13:38

I have a similar [DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/STM32F10x connection via USART problem&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E]problem. I tried to use my eval board(STM32F107) in DFU mode and write internal flash with DFuSe. Connected board to PC via USB. And PC viewed unknown device with PID=0000&VID=0000! But need VID=0483 & PID=DF11 as in STDFU.inf.

May be board have a bad bootloader and problem with USART connection associated with this?

Excuse me for my English.
Tomas DRESLER
Associate II
May 17, 2011
Posted on May 17, 2011 at 13:38

The date code 961 tells that this chip comes from very first batch and the bootloader is not present. Contact your ST marketing for replacement.

Tomas DRESLER
Associate II
May 17, 2011
Posted on May 17, 2011 at 13:38

Check whether you've downloaded the DFU for proper family. Next, does your board implement the USB D+ disconnect? I remember on some boards the disconnect had a jumper, that permanently shortcutted the transistor and the USB host recognized the device instantly & too early before DFU code booted.

tkjmail2
Associate III
May 17, 2011
Posted on May 17, 2011 at 13:38

If the issue isn't that there is no bootloader in the chip, then I've found out that I had to lower the connection speed to 57600 bps, as it gave me connection errors most of the time when I was using 115200 bps!

Tomas DRESLER
Associate II
May 17, 2011
Posted on May 17, 2011 at 13:38

Nope, date codes before 937 (year [20x]9, week 37) have no bootloader. Ask your ST marketing for replacement. Btw. 961 is obviously not a valid week in any year, it's a pilot version.

aleksey
Visitor II
May 17, 2011
Posted on May 17, 2011 at 13:38

Chip on my board marked as STM32F107VCT6 Z 99056 VC MYS99 923. Does bootlader present in this version?

USB D+ connected. The board work correctly with my firmwares which use HID and CCID protocol. I have a problem when board booting from system memory only. USART connection don't work too.

ramadevi
ramadeviAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 13:38

Hi,

Thanks for the replies.It took sometime to get another board and now I have STm32 board with 923 marking. But I am able to use flash loader demo and write the kernel bootloader to the flash.

When I connect the board to PC through a USB, it is not detected.'Found new hardware' is not working and 'Add new hardware' feature not lists the STM board.

My settings:Boot mode in User flash and JP14 in connected mode.

Any help is much appreciated.

Thanks a lot.

aleksey
Visitor II
May 17, 2011
Posted on May 17, 2011 at 13:38

Edison, thanks for your answers.

I dumped memory 0x1fffb000-0x1ffff7ff (system memory area). It's contains some code. In this code VID (0x0483) have offset 0x1fffeae8 and PID (0xdf11) have offset 0x1fffeaea.

Conclusion: chip have bootloader, but it don't work!
ramadevi
ramadeviAuthor
Associate II
May 17, 2011
Posted on May 17, 2011 at 13:38

Is there a way to flash the board using ST-Link JTAG and KEIL/IAR IDE? How can we make use of this board?

I am little confused about the usage?

aleksey
Visitor II
May 17, 2011
Posted on May 17, 2011 at 13:38

Hi,

STM support replied to me about this problem.

STM

32

F

107

VCT

6 with data code before 941 have a bootloader's problem with USB and USART connections.