Skip to main content
nj_boelskov
Associate III
Jun 10, 2008 4:03 AM UTC
Question

Error: target CPU does not support ARM mode

Posted on June 10, 2008 at 06:03

Error: target CPU does not support ARM mode

    This topic has been closed for replies.

    6 replies

    jj_it
    Associate II
    May 17, 2011 10:36 AM UTC
    Posted on May 17, 2011 at 12:36

    Some time back we contacted CodeSourcery

    re: STM32. Recall that it was ''under consideration.''

    Yesterday their site still did not include STM32

    under supported devices...

    nj_boelskov
    Associate III
    May 17, 2011 10:36 AM UTC
    Posted on May 17, 2011 at 12:36

    ...and when I try to use the GNUARM toolchain i get the errormessage:

    error: bad value (cortex-m3) for -mcpu= switch

    so the GNUARM toolchain do not support cortex-m3??

    [ This message was edited by: nj_boelskov on 06-06-2008 13:28 ]

    nj_boelskov
    Associate III
    May 17, 2011 10:36 AM UTC
    Posted on May 17, 2011 at 12:36

    Hey

    I am trying to use CodeSourcerys toolchain in uVision, and used the guide (see attachment) to do the setup in uVision. It looks simple, but every time I try to compile a project, I get the following erro message for all files:

    target CPU does not support ARM mode

    The target CPU is set to STM32F103RB and i'm on the MCBSTM32 kit.

    Any ideas about what the problem could be?

    [ This message was edited by: nj_boelskov on 06-06-2008 13:20 ]

    nj_boelskov
    Associate III
    May 17, 2011 10:36 AM UTC
    Posted on May 17, 2011 at 12:36

    Made a new linkerfile (ld) and now I can Compile the project.

    nj_boelskov
    Associate III
    May 17, 2011 10:36 AM UTC
    Posted on May 17, 2011 at 12:36

    Hi

    I checked a box called ''Compile Thumb Code'' and -mthumb was added to the Compiler control string. It seems to help, but another warning came up.

    it ''cannot find entry symbol _start''

    ...and I understand that, because I have no _start in my startup.c or vector.c (I got them from this forum) so maybe my startupcode are wrong.

    I looked at this

    http://www.st.com/mcu/forums-cat-6445-23.html

    , but I can't realy finde out which files to include into my project. Can I use some of Lanchons files, or do I have to finde some others?

    [ This message was edited by: nj_boelskov on 09-06-2008 11:10 ]

    sjo
    Associate III
    May 17, 2011 10:36 AM UTC
    Posted on May 17, 2011 at 12:36

    The application note works fine, you will have to check your setup.

    For a start the clue is ''target CPU does not support ARM mode''.

    This is quite correct as it is a cortex_m3 and only supports thumb2.

    Also currently GNUARM does not support armv7 (cortex_m3).

    Regards

    sjo