Skip to main content
Andrew Neil
Super User
November 10, 2016
Question

STLink Command Line - connect & stay connected?

  • November 10, 2016
  • 2 replies
  • 1318 views
Posted on November 10, 2016 at 15:59

Is there a way to get the STLink Command Line utility to connect to the target and stay connected?

If I issue the -C (Connect) command, it does connect - but then immediately disconnects & exits back to the Windows command prompt.

How do I get it to

stay

connected - so that I can enter further commands interactively?

Is it possible?

#stlink-st-link
This topic has been closed for replies.

2 replies

slimen
Visitor II
November 15, 2016
Posted on November 15, 2016 at 13:40

Hi,

- The [HOTPLUG] option allows to connect to the target without halt or reset.

For more details, refer to the 

http://www.st.com/content/ccc/resource/technical/document/user_manual/e6/10/d8/80/d6/1d/4a/f2/CD00262073.pdf/files/CD00262073.pdf/jcr:content/translations/en.CD00262073.pdf

 in the ''STM32 ST-LINK utility command line interface (CLI)'' section.

Regards

Andrew Neil
Super User
November 15, 2016
Posted on November 15, 2016 at 14:48

Sorry, that's not what I was asking at all.

I'm talking about having the Command-Line interface remain connected to the target.

But ST Support confirms this is not possible: the CLI will just execute one command, and then disconnect form the Target.

But they did add:

you can chain the commands in the same command line and add -pause in between to request user to proceed for next command.

I haven't tried that - I managed to achieve what I want using OpenOCD ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.