Skip to main content
stmail
Associate
March 19, 2009
Question

Receiving blocks of data using SPI and DMA

  • March 19, 2009
  • 1 reply
  • 540 views
Posted on March 19, 2009 at 13:04

Receiving blocks of data using SPI and DMA

    This topic has been closed for replies.

    1 reply

    stmail
    stmailAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:07

    I want to receive 48bit blocks of data using the STM32 as a SPI slave. The following code works fine:

    (SPI2_DR_Address=SPI data register,SPI_RxBuffer_size=6

    [...]

    DMA_InitStructure.DMA_PeripheralBaseAddr = (u32)SPI2_DR_Address;

    DMA_InitStructure.DMA_MemoryBaseAddr = (u32)g_SPI_RxBuffer.list;

    DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;

    DMA_InitStructure.DMA_BufferSize = SPI_RxBuffer_size;

    DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

    DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

    DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;

    DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;

    DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

    DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh;

    DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;

    DMA_Init(DMA1_Channel4, &DMA_InitStructure);

    SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

    SPI_InitStructure.SPI_Mode = SPI_Mode_Slave;

    SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;

    SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;

    SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;

    SPI_InitStructure.SPI_NSS = SPI_NSS_Hard;

    SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_LSB;

    SPI_Init(SPI2, &SPI_InitStructure);

    [...]

    But I think it's rather inefficient as there are six bus accesses.

    I tried to change it to the the following:

    [...]

    DMA_InitStructure.DMA_BufferSize = 3;

    [...]

    DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

    DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

    [...]

    SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b;

    [...]

    Should only need three accesses, but instead of the real data, I only received zeroes...

    Any reasons or ideas for that strange behaviour?