Skip to main content
gioacchino03
Associate
March 10, 2009
Question

Load multiple instruction timing

  • March 10, 2009
  • 4 replies
  • 896 views
Posted on March 10, 2009 at 13:57

Load multiple instruction timing

    This topic has been closed for replies.

    4 replies

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:05

    Hi gioacchino03,

    Quote:

    .... so it seems that every load instruction takes a minimum of three CPU cycles: 1 AHB cycle (arbitration) + 2 CPU cycles (execution)

    The contex-m3 can execute a load multiple instructions in (nReg + 1) cycles, where nReg is the number of registers loaded. In the STM32, due to bus arbitration, this value is (2 x nReg +1) cycles instead.

    Could you let me know how you did the calculation ? I suggest you To check it on real STM32 silicon, you can run a small piece of code in assembly having some Multiple loads and then share with us the timing cycles.

    Cheers,

    STOne-32.

    gioacchino03
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:05

    Hello!

    I have noted some differences between cortex-m3 theretical performnces and stm32 true performnces when executing load instructions...

    The appliation note abaut the stm32 DMA you can find at this link:

    http://www.st.com/stonline/products/literature/anp/13529.htm

    tells that the CPU have to pay an AHB cycle when exsecuting load instruction

    due to bus arbitration whit the DMA, so it seems that every load instruction takes a minimum of three CPU cycles:

    1 AHB cycle (arbitration) + 2 CPU cycles (execution)

    The contex-m3 can execute a load multiple instructions in (nReg + 1) cycles, where nReg is the number of registers loaded. In the STM32, due to bus arbitration, this value is (2 x nReg +1) cycles instead.

    Can anyone confirm my idea?

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:05

    Hi,

    Excellent job ! So, You confirmed that STM32 is behaving exactly as stated in the theory of the instruction timing as defined by ARM Cortex-M3 core :) even the flash is with 2 wait states and CPU running at 64Mhz , let's try now when the DMA is enabled..

    Cheers,

    STOne-32.

    gioacchino03
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:05

    Hello,

    tanks for your interest... My previous post was based on a simulation whit Keil uVision. Now I have done some test on real hardware:

    My settings are:

    * external crystal 4MHz

    * PllMul = 16

    * Pre-fetch buffer whit 2 wait-states

    * AHBPRE = 1

    This leads:

    * core cycle time = (1/(4Mhz * 16)) = 15.6ns

    STM32 taken about 11us to execute 100 instructions like this:

    LDMIA SP,{R2,R3,R4,R5,R6,R7}

    so each LDM instruction takes (11us/100) = 110ns = 7 x 15.6ns !

    Conclusion: the minimum (DMA disabled) number of cycles to transfer n word from memory to registers is n+1 ! :D