Skip to main content
tboss
Associate
March 15, 2010
Question

FMI Troubles

  • March 15, 2010
  • 8 replies
  • 1735 views
Posted on March 15, 2010 at 12:40

FMI Troubles

This topic has been closed for replies.

8 replies

robosoft2
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:00

Hi ,

I have exactly the same problem. Is this problem solved ?

Pls let me know.

willie
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:00

This is one of several FUQs (Frequently Unanswered Questions) to ST.

This (as explained in the newest Flash Programming manual) can be

prevented by executing the following instructions:

    MOV r0, #0x40000

    MCR p15,0x1,r0,c15,c1,0

The problem is that if these instructions are executed at any time except

during the initialization the ARM throws an Undefined instruction fault.

I have found that a delay solves the problem, one just have to be careful

that the compiler does not optimise the code away.

whh

robosoft2
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:00

Here is my code to erase sector7 from bank0. This code is compiled to execute in RAM.

When I execute the code step by step in my debugger (Keil JLINK) it works.

Without debugger it never returns...

void Erase(void)

 

{

 

  volatile long Time_Out = 0;

 

  volatile vu32 FMI_Sector = FMI_B0S7;

 

   /* Write an erase set-up command to the sector */

 

   *(vu16 *)FMI_Sector = 0x20;

 

   /* Write an erase confirm command to the sector */

 

   *(vu16 *)FMI_Sector = 0xD0;

 

   /* Wait until operation compeletion */

   while((!((*(vu16 *)FMI_Sector) & 0x80))&&(Time_Out < TIMEOUT ))

 

   {

 

     Time_Out ++;

 

   }

 

   *(vu16 *)FMI_Sector = 0x50;

 

   /* Write a read array command */

 

   *(vu16 *)FMI_Sector = 0xFF;

 

}

regards

Luc

Tesla DeLorean
Guru
May 17, 2011
Posted on May 17, 2011 at 10:00

The presented code screams for the use of the volatile type.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
May 17, 2011
Posted on May 17, 2011 at 10:00

So much for an appropriate use of volatile.

 

 The following would be a more consistent usage

 

 

  long Time_Out = 0;

 

  volatile vu32 *FMI_Sector = (volatile vu32 *)(FMI_B0S7);

 

   /* Write an erase set-up command to the sector */

 

   *(volatile vu16 *)FMI_Sector = 0x20;

 

   /* Write an erase confirm command to the sector */

 

   *(volatile vu16 *)FMI_Sector = 0xD0;

 

   /* Wait until operation compeletion */ ...

Or more effectively

void Erase(void)

 

{

 

  long Time_Out = 0;

 

  volatile vu16 *FMI_Sector = (volatile vu16 *)(FMI_B0S7);

 

   /* Write an erase set-up command to the sector */

 

   *FMI_Sector = 0x20;

 

   /* Write an erase confirm command to the sector */

 

   *FMI_Sector = 0xD0;

 

   /* Wait until operation compeletion */

   while((!((*FMI_Sector) & 0x0080))&&(Time_Out < TIMEOUT ))

 

   {

 

     Time_Out ++;

 

   }

 

   *FMI_Sector = 0x50;

 

   /* Write a read array command */

 

   *FMI_Sector = 0xFF;

 

} >>Do you still use the STR912 ? I hate this device !

Life would likely be easier if you used the library code, or were more familiar with C and the tool chain.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
robosoft2
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:00

Hi Paolo,

Thanks for response.

It stil does not work. Erasing a sector from BANK0 is no problem, erasing a sector in BANK1 does not work, except step by step with JTAG debugger.

Do you still use the STR912 ? I hate this device !

Kind regards

Luc

paolo239955_stm1_stmicro
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:00

Hi,

in the past i used STR912FA and i solved the problem in this way:

void EraseSector(u32 Sector)

{

  /*

slowed down to write

la flash (FMI @48Mhz) */

  SCU_FMICLKDivisorConfig(SCU_FMICLK_Div2);

  /* Clear */

  FMI_WriteProtectionCmd(Sector, DISABLE);

  FMI_EraseSector(Sector);

  FMI_WaitForLastOperation(FMI_BANK_1);

  FMI_WriteProtectionCmd(Sector, ENABLE);

  /* Full speed (FMI @96Mhz) */

  SCU_FMICLKDivisorConfig(SCU_FMICLK_Div1);

 

}

All FMI routine of ST Library are execute in RAM.

In FMI_WaitForLastOperation disable PFQBC see errata

__ramfunc u8 FMI_WaitForLastOperation(vu32 FMI_Bank)

{

  u32 Time_Out = 0;

 

  /* Write a read status register command */

  *(vu16 *)(FMI_Bank) = 0x70;

  /* Disable PFQBC (see Errata pag 5) */

  SCU->SCR0 &=~0x1;

  /* Wait until operation compeletion */

  while((!((*(vu16 *)FMI_Bank) & 0x80))&&(Time_Out < TIMEOUT ))

  {

    Time_Out ++;  /* Time Out */

  }

  /* Write a read array command */

  *(vu16 *)FMI_Bank = 0xFF;

  /* Enable PFQBC */

  SCU->SCR0 |=0x1;

 

  if (Time_Out == TIMEOUT)

  {

    return FMI_TIME_OUT_ERROR;

  }

  else

  {

    return FMI_NO_TIME_OUT_ERROR;

  }

}

I hope

it is

useful

Paolo

robosoft2
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:00

Thanks for reply. It seems to be OK now.

>>Do you still use the STR912 ? I hate this device !

>>Life would likely be easier if you used the library code, or were more familiar with >>C and the tool chain.

I use the library code. I made a *.lib and linked it in my code. The part 91x_FMI was compiled to be executed in RAM. This does not work. When I compile the 91x_FMI files separate and link it in my code, it does work.

I have been programming devices for over 20 years in C. I use this toolchain for NXP LPC2470, SAMSUING S3C2440 without problems. PIC16, PIC32 is a pleasure to work with...

And, no, I think my life would be easier if the erratasheet is a bit smaller ...

So, lets say I do not hate this device, but I never gonna love it !

Thanks anyway

Luc