Skip to main content
yagov
Associate II
April 6, 2010
Question

The problem to init LCD glass controller on STM8L152C6

  • April 6, 2010
  • 2 replies
  • 1089 views
Posted on April 06, 2010 at 13:05

The problem to init LCD glass controller on STM8L152C6

    This topic has been closed for replies.

    2 replies

    yagov
    yagovAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 15:07

    It was a problem of board. It was damaged. Project works well on another one

    mozra272
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:07

    .ExternalClass57FC0A59E9854DD989D505606BC1AF5E p.MsoNormal, .ExternalClass57FC0A59E9854DD989D505606BC1AF5E li.MsoNormal, .ExternalClass57FC0A59E9854DD989D505606BC1AF5E div.MsoNormal {margin:0in;margin-bottom:.0001pt;font-size:12.0pt;font-family:'Times New Roman';} @page Section1 {size:8.5in 11.0in;margin:1.0in 1.25in 1.0in 1.25in;} .ExternalClass57FC0A59E9854DD989D505606BC1AF5E div.Section1 {page:Section1;}

    Hi Yagov,

    When using the STM8L1526-EVAL make sure that the LCD daughter board MB821 is connected on the LCD position.

    Regards

    mozra